AnsweredAssumed Answered

What is the phase noise of HMC439 at 10Hz offset for 10 MHz pdf?

Question asked by mins on Jun 6, 2016
Latest reply on Aug 31, 2016 by dmailloux

Hello,

 

I will use HMC439 in a 100MHz clock generator application with 10 MHz pfd comparison frequency and i need phase noise data at 10Hz offset. In the datasheet it starts at 100Hz and I see a peak near 100 Hz. How is its behaviour below 100Hz? Also can I assume 10 dB decrease in 100MHz phase noise data when using it for 10MHz operation?

 

Thank you,

 

Mustafa

Outcomes