AnsweredAssumed Answered

OSD for ADV7625

Question asked by SamLiao on Jun 6, 2016
Latest reply on Jul 12, 2016 by JeyasudhaMuthuPerumal

Dear ADI:

 

     Now ,I use ADV7625 to design a product. I want to use the OSD function. I'm ready to use BF70x  to control ADV7625 through IIC/SPI, I read the Blimp_User_Manual and Blimp_ADV7625_Framework_User_Manual, But i still have some questions:

 

     Q1: I must need a Extend SPI FLASH to store ddr2_dump.bin ,hasn't it??

 

     Q2: With Blimp ,there generate a pile of files,if i control ADV7625  through IIC/SPI, which files are needed?just the files under floder fireware??

 

Thank u very much &BR!!

 

 

 

 

 

 

 

 

Outcomes