AnsweredAssumed Answered

What is the allowable clock frequency range for the USB0_CLKIN clock input on the BF707?

Question asked by larrabure on Jun 3, 2016
Latest reply on Jun 8, 2016 by JoeT


The datasheet states that the USB XI frequency is 24Mhz, and only 24 MHz.  However, USB XI is not mentioned anywhere else in the datasheet or the hardware manual.  Can USB CLKIN only take in a 24MHz?  Or is there some range of acceptable frequencies?

Outcomes