AnsweredAssumed Answered

Communication via USB between two BF526s

Question asked by Mack on Jul 23, 2011
Latest reply on Jul 26, 2011 by PrasanthR

Hello,

 

I am going to start designing a system which consists of two BF526-based boards.  The two boards will be linked each other via USB.

What I want to know are

  1. for usb communication, should one operate as a host and the other operate as a device?

      1) If yes, could I get USB host example?

 

  2. is there a way to make two BF526s communicate thru USB with no need of usb host/device configuration?

 

  3. Is there any other good way to transmit as high date rate as usb does?

 

Best Regards,

Mack.

Outcomes