AnsweredAssumed Answered

Loading the internal BF504F FLASH in production

Question asked by ByTor on Jul 22, 2011
Latest reply on Nov 4, 2011 by hackfin

I was wondering if there is a standalone application available for programming the internal FLASH that does not require the VisualDSP++ IDE.

 

I have a BF504F application which executes some code directly from the internal FLASH and some from SRAM.  In development, I use the VisualDSP++ IDE to load the FLASH code at 0x2002 0000 and the FLASH programming tool to load the SRAM code in the .ldr file at 0x2000 0000 as described in http://ez.analog.com/docs/DOC-1274.

 

Is anyone aware of a standalone utility that could be used in production?  It seems a waste to purchase another VisualDSP++ seat just to program parts.

 

-Thanks

Outcomes