AnsweredAssumed Answered

AduM4135 Absolute Maximum Ratings

Question asked by Prospy on May 28, 2016
Latest reply on May 28, 2016 by RSchnell

Hi,

 

There Is something that I don't understand about the ADum4135 Absolute Maximum Ratings (page 7 data sheet). Here the minimum Vgate_sense is -0.3V but if the Miller Clamp is not used then I have to tie GATE_SENSE to VSS2 and VSS2 could be -15V.

 

 

So I thing the absolute maxim rating for GATE_SENSE is VSS2.

Same thing about absolute rating in Vout_off.

Is this right?

Thanks

Outcomes