AnsweredAssumed Answered

ADV7619 settings for 4k1K @60Hz

Question asked by gubuyu on May 26, 2016
Latest reply on Jun 20, 2016 by JeyasudhaMuthuPerumal


Hi,

I am using an ADV7619 to receive 3840*1080 @60Hz HDMI signals. Its' pixel bus is configured in 2x24-bit 4:4:4 SDR interleaved mode. The pixel bus is connected to an FPGA.

I have a problem, the ADV7619 is not able to produce correct DATA output.When value of Video source is 165(white,RGB=0xA5A5A5),the device  output is not fixed vlaue 0xA5A5A5A5A5A5.sometimes is 0xA6A5A5A6A5A5 or 0xA5A5A6A5A5A6 or 0xA5A6A5A5A6A5.

I try to change vlue of 0x19 register of IO Map,from (0x98, 0x19, 0x80) //LLC DLL phase  to  (0x98, 0x19, 0x9F).

But it has no effect.

I use the script "ADV7619-VER.1.9c.txt" to configure the ADV7619.

##03 HDMI Input to ADV7619, Input Pixel Frequency > 170MHz ##

:03-01 RGB 444 In - 2x24-bit RGB 444 Out - For use up to 4k2k:

98 FF 80 ; I2C reset

98 F4 80 ; CEC

98 F5 7C ; INFOFRAME

98 F8 4C ; DPLL

98 F9 64 ; KSV

98 FA 6C ; EDID

98 FB 68 ; HDMI

98 FD 44 ; CP

68 C0 03 ; ADI Required Write

98 00 19 ; Set VID_STD

98 01 05 ; Prim_Mode =101b HDMI-Comp

98 02 F2 ; Auto CSC, RGB out, Set op_656 bit

98 03 54 ; 2x24 bit SDR 444 interleaved mode 0

98 05 28 ; AV Codes Off

98 06 A0 ; No inversion on VS,HS pins

98 0C 42 ; Power up part

98 15 80 ; Disable Tristate of Pins

98 19 83 ; LLC DLL phase

98 33 40 ; LLC DLL MUX enable

98 DD 00 ; ADI Required Write

98 E7 04 ; ADI Required Write

4C B5 01 ; Setting MCLK to 256Fs

4C C3 80 ; ADI Required Write

4C CF 03 ; ADI Required Write

4C DB 80 ; ADI Required Write

68 C0 03 ; ADI Required write

68 00 08 ; Set HDMI Input Port A (BG_MEAS_PORT_SEL = 001b)

68 02 03 ; ALL BG Ports enabled

68 03 98 ; ADI Required Write

68 10 A5 ; ADI Required Write

68 1B 00 ; ADI Required Write

68 45 04 ; ADI Required Write

68 97 C0 ; ADI Required Write

68 3E 69 ; ADI Required Write

68 3F 46 ; ADI Required Write

68 4E FE ; ADI Required Write

68 4F 08 ; ADI Required Write

68 50 00 ; ADI Required Write

68 57 A3 ; ADI Required Write

68 58 07 ; ADI Required Write

68 6F 08 ; ADI Required Write

68 83 FC ; Enable clock terminators for port A & B

68 84 03 ; FP MODE

68 85 10 ; ADI Required Write

68 86 9B ; ADI Required Write

68 89 03 ; HF Gain

68 9B 03 ; ADI Required Write

68 93 03 ; ADI Required Write

68 5A 80 ; ADI Required Write

68 9C 80 ; ADI Required Write

68 9C C0 ; ADI Required Write

68 9C 00 ; ADI Required Write

End

 

Can you give me some advice please?

I do not have evaluation board.

 

Thanks,

Best regards.

Outcomes