AnsweredAssumed Answered

Input Voltage Range for ADR425BRZ

Question asked by SureshSurya on May 25, 2016

Hi,

 

     As per the datasheet of ADR425BRZ, the device can  be operated with a input range of +7V to +15V. But in the specification section of  datasheet the recommended Vin is +7V to +15V. Absolute maximum rating of the Vin pin is +18V. So, Kindly advise me regarding operating with the input range of +14.5 V to +15.5 V.

 

Thanks in advance,

 

Surya

Outcomes