AnsweredAssumed Answered

Can the no-os software be used to calibrate Tx channel 2 for the ad9361?

Question asked by BB-8 on May 24, 2016
Latest reply on Jun 6, 2016 by BB-8

I don't see anything in the software that differentiates between transmitting channel 1 and channel 2 other than "phy->pdata->rx2tx2".  I want to pick my channel based on frequency band, but when I switch rx2tx2 to select channel 2, the channel (and therefore port) changes appropriately, but I get a much worse looking result (carrier suppression is terrible--the carrier is around -15dB compared to -48dB on channel 1), making me think that calibration isn't happening properly for that channel, but I can't find anything in the calibration code that specifies channel.  Is channel 2 getting calibrated at all?

Outcomes