AnsweredAssumed Answered

ADV7604- Any register to find mismatch between Incoming & Configured resolution

Question asked by Prabul on May 23, 2016
Latest reply on May 23, 2016 by JeyasudhaMuthuPerumal

Hi,

I am using ADV7604 in the following mode.

Video Input for ADV7604   : Analog RGB with discrete Sync (AIN 7,8,9 for RGB) and

Video Output by ADV7604 : 24 bit RGB with discrete Sync.

Is there any way to find if there is a mismatch between input resolution and the configured resolution?

I am looking for internal registers of ADV7604 which can be accessed through I2C interface from which i can infer if there is a mismatch between incoming resolution and the configured resolution.

Outcomes