AnsweredAssumed Answered

NoOS Capture Scripts don’t run

Question asked by kNl on May 20, 2016
Latest reply on May 20, 2016 by DragosB

Hello,

My setup consists of a zynq702 and an FMCOMMS5 eval board. I ‘m trying to collect the I/Q captured data of the no os example https://github.com/analogdevicesinc/no OS/tree/master/ad9361/sw using the scripts from here https://github.com/analogdevicesinc/noOS/tree/master/ad9361/scripts/fmcomms5_zc702

 

But the capture.bat terminates without storing the data to the .csv file.

I just downloaded the files and stored them to the same folder. Is there any specific folder that they should be stored?

I only modified the location of my Xilinx installation directory and ran the capture.bat. The zynq702 is connected to the PC through the USB cables too. When I run the example with Vivado and SDK there is no problem at all.

I also tried to run the script in Windows 10 and Windows 7. problem.png

I would appreciate it if you could help,

Katerina.

Outcomes