AnsweredAssumed Answered

Disable free run on ADV7619 and Validate TMDS/Tx core On ADV8005

Question asked by prasannakarthik on May 20, 2016
Latest reply on May 23, 2016 by JeyasudhaMuthuPerumal

We are trying to use below setting for disabling free run,

0x44 0xba 0x00 // HDMI_FRUN_EN

0x44 0xbf 0x16 // CP_FORCE_FREERUN

0x98 0x01 0x02 //VID_STD[5:0]: 0x02

0x98 0x00 0x06 //PRIM_MODE[3:0]: 0x06

Here is the vsp version:

********************************************************************

  ADI VSP AVR Application Ver V1.90.2

  PLATFORM: EVAL-ADV8005-SMZ

  HDMI-RX:  ADV7619 Rev 0x20c1

  HDMI-TX:  ADV8005 Rev 0x6083 without Rovi

  Created:  May 18 2016 At 11:47:47

********************************************************************

With this setting, we still see a 480p signal in TX1.

Please provide a method to validate to free run setting apart from checking the presence on TX1.

Outcomes