AnsweredAssumed Answered

ADV7611 output to BF609

Question asked by mutgan on May 19, 2016
Latest reply on May 26, 2016 by mattp

Hello,

After solving the issue with the ADV7611 input ADV7611 without any HPA and EDID , now I am having trouble with getting the image to PPI0 of BF609 ( custom board ) . I can detect the DVI input signals without any problems and I can see the 74.250 MHZ clock on the LLC which is connected to PPI CLK ( Vpp = 1.7V ).  I cannot read the data in BF609.

 

What should I check to eliminate the hardware issue?

I have selected the EPPI0 in Pin Multiplexing tool. I am modifying  the Video Decoder EI3 board frame capture example.

 

Thank you in advance,

 

Best,


Hazar

Outcomes