AnsweredAssumed Answered

require IC for swicthing of base band signals in freq range DC-20MHz, with input and output levels upto 9 dBm at 50 ohms load. Is AD8174 right choice?

Question asked by shikhabel on May 20, 2016
Latest reply on Jun 23, 2016 by shikhabel

Whether IC AD8174 suitable for following requirements?

 

Base band switching IC in freq range DC- 40MHz

Input level: +5dBm at 50 ohms

Output drive level: +9dBm at 50 ohms

Slew rate better than 500V/s

High input to output isolation within the band

Outcomes