AnsweredAssumed Answered

operating the USB driver

Question asked by jacob on Jul 20, 2011
Latest reply on Jul 21, 2011 by CraigG
Branched to a new discussion

Hi,

I am using the BF548 Evaluation Board.

I want to transfer data from my PC to the Device and from the Device to the Pc using the USB controller (with the usb otg connector).

 

should i define the device an audio device or a mass storage device?

 

then, i want to load and fetch data with matlab.

 

i have operated the "bulk_redirect_io_app" program, but the corresponding application does not work.

i get the folloing error at the command line: "-h is not recognized as an internal or external command".

 

what do you think i should do?

how can i operate an expamle to see how can i use the USB drivers?

 

Thanks!

jacob

Outcomes