AnsweredAssumed Answered

The Clkin for the PCG on ADSP-SC589

Question asked by dell-jin Employee on May 17, 2016
Latest reply on May 19, 2016 by dell-jin

Dear All:

     The input clock of PCG can be selected from the CLKIN, but there are two CLKINs on the ADSP-SC589, which is the right input to the PCG module? or we can choose one from the clkin0 and clkin1. there is no detaild description in  the sc58x's HRM. can anybody help to clarify it ?

    Thanks..

 

Regards

Dell

Outcomes