AnsweredAssumed Answered

Can Trim Reg in ADP1048 be programmed when loading register settings?

Question asked by dmalane on May 11, 2016
Latest reply on May 13, 2016 by dmalane

Hello,

 

I'm using the adp1048 for a interleaved PFC application. In the prototype I configured the register and board settings that everything was running smooth. I saved these Settings using the button in the GUI. Today I had a got a second hardware and I loaded the previous saved Settings to the ADP1048. I doubled checked the loaded settings and there was a mismatch between the TRIM values. I used the spy window to check whether the TRIM Registers are written or not and there I could see that no TRIM-values are written when loading the register settings. Is this the expected behaviour? How can I change the trim values without doing it manually?

Would be very thankful for help.

 

Regards,

Dominic

Outcomes