AnsweredAssumed Answered

ADG858 for USB?

Question asked by Vala on May 10, 2016
Latest reply on Jul 4, 2016 by mayp

Hi,

 

Could you please confirm if I can use two channels of ADG858 for USB data lines? I checked the important specifications (like On resistance, on resistance flatness, matched on resistance, bandwidth) for this device and compared with some devices which are recommended by AD for USB applications, such as ADG787. It seems that the USB requirements are satisfied by ADG858 too. But there is nothing mentioned about USB in ADG858's data sheet. I didn't find an eye diagram in it either.

 

The reason that I prefer to use ADG858 is that I need its four matched channels and I will be using two of them for USB data lines. Could anyone tell me if I am going wrong about this?

Outcomes