AnsweredAssumed Answered

End resistance

Question asked by stromar89 on May 10, 2016
Latest reply on May 16, 2016 by msamera

Hello,

 

I'm using AD8403 50kOhm and 10kOhm variable resistors for my application, but the maximum resistance I can get is around 43kOhm for 50kOhm resistors and around 9200Ohm for 10kOhm resistors. At the beginning of development of aplication I've used AD5206 50kOhm variable resistors. With those I can get up to around 51kOhm.

So I wonder why is there such difference even though the only difference should be the accuracy?

 

Regards,

Bojan

Outcomes