AnsweredAssumed Answered

AD5271 Confirm the datasheet

Question asked by ishino@fujiele.co.jp on May 10, 2016
Latest reply on May 10, 2016 by msamera

Hello, ADI team.

My customer considering to use AD5271. He has the doubt to datasheet described. In datasheet p19, Table11,

command7 , there is no description of the D3 is in error.To determine from Table 13 and 14, it seems like the need to select 1 in the part of DB3(C3) when writting to the command register.

What kind of the reason is that this part has become a X "especially don't care" in Table 11?

Outcomes