AnsweredAssumed Answered

A Complete Example in MATLAB

Question asked by Manos on May 6, 2016
Latest reply on Oct 31, 2016 by ACozma

Hello,iam trying to execute a matlab example which can be found in :  LTE Transmitter and Receiver Example [Analog Devices Wiki]

My setup consists of a zynq706 and an FMCOMMS5 eval board.

I downloaded all the files regfarding the LTE example and the Libio inteface from the github : MathWorks_tools/hil_models/LTE_MATLAB at 2015_R1 · analogdevicesinc/MathWorks_tools · GitHub .

 

I have downloaded and installed the latest image of linux.

When i run the ad9361_LTE.m file in matlab i keep getting the following error message in the command line:

Struct contents reference from a non-struct array object.

Error in ad9361_LTE (line 79)

s.writeFirData(fir_data_file);

 

and a GUI with an error message saying : could not connect to the IIO Server.

 

Moreover, i dont get which is considered to be the server, the host device(pc) or the target(FMCOMMS5)?

 

It should be plug and play considering that i just had to download the files and run the example.

Any ideas of what can be wrong?

Outcomes