AnsweredAssumed Answered

AD9272

Question asked by Ingeniero7 on Jul 16, 2011
Latest reply on Jul 19, 2011 by ginak

Hello, i´m using chip AD9272, I have a question...

 

I only want to use one channel, and i don´t know if i have to connect all the pins of the supply ( AVDD1 and AVDD2) or if  i can connect only some of them , that is, i´m using the channel A, so i suppose that i have to connect the pin 54 and 55, and the pin 25 for the clock , the pin 86 for the circuit GAIN+- , and the pin 26 and 47 for digital outputs..... but maybe , i´m wrong ....

 

Thanks, for the help...

Outcomes