AnsweredAssumed Answered

Set Reset Edge Triggered Latch

Question asked by Brettcoupe on May 3, 2016
Latest reply on May 28, 2016 by Brettcoupe


Hi . I Need a method to Set a LATCH to "0"  when Signal A  goes below an adjustable threshold.

and only reset it to "1" when a Different signal Goes above a Different threshold.

The problem I appear to be having is that i need Edge triggering.

The purpose is to make a detector that has fast release to "Hold - freeze" the output level  of a slow attack detector. and do not release this "hold" until the level of the slow attack detector has become equal to the "frozen" level.

 

 

Another way I maybe able to solve this is to have  a detector A that has fast release But has  the Same SLOW Attack speed, as detector B's Decay speed.

I hope this makes sense?

Thanks

Brett

Outcomes