AnsweredAssumed Answered

Linux Kernel panic when xilinx axi dma is enabled on Zynq zc706 running ADI kernel

Question asked by abmartin on May 2, 2016
Latest reply on May 10, 2016 by abmartin

Hi,

I am working on the zynq zc706 board connected with FMCOMMS2-EBZ, running Linux Kernel(3.19.0) provided by Analog Devices(2014_R2). I am using the ADI AXI DMAC for data transfer.

But when I try to add the Xilinx AXI DMA Engine driver into the Linux Kernel provided by ADI(2014_R2). I am following the steps from http://www.wiki.xilinx.com/DMA+Drivers+-+Soft+IPs and I boot up the system using the new uImage and devicetree, I am seeing Kernel Panic.

Could anyone tell me where I could be going wrong. I have attached the kernel log

Outcomes