AnsweredAssumed Answered

ADXL312's temperature range

Question asked by henry-tang on Apr 28, 2016
Latest reply on May 3, 2016 by henry-tang

Dear Sir/Maiden,

 

I have a question about ADXL312's datasheet, can ADI please kindly help to check it?

 

ADXL312's datasheet shows Temperature range in Absolution Maximum rating section.

It shows the range should be from −40°C to +125°C when Powered.

 

1.png

 

May I ask what Temperature range (Powered) means here?

Is Ambient Operating Temperature Range (TA) or Junction Temperature (TJ)?

In the same datasheet's last page, it shows Temperature range it's from −40°C to +105°C.

And then what does the temperature range here means?

 

2.png

 

Any suggestion or opinion is highly appreciated!

 

Henry

Outcomes