AnsweredAssumed Answered

High-speed communication with host pc

Question asked by Ronen on Apr 28, 2016
Latest reply on Apr 28, 2016 by ACozma

Hi there.

 

Im currently using the zc702 and AD-FMCOMMS3 boards. i've been using these in order to process

a real-time video filmed by a webcam.

 

To help with this process, I first tried transmitting a photo that was changed to a .bit file and then dumped to

 

memory manually, and it worked.

 

Howerver, this did not work with the processing of a real-time video, as I had been dumping the bit files manually

and not via C source.

 

As a solution I used matlab and it worked, howeer it was extremely slow.(serial communication / 115kbits/s)

 

I really needed to find a method that allows SDK(C source) to receive an image directly(or via host pc) by usb webcam

in C source. Are there any functions that allow SDK to receive information from the host in high speed?

 

Regares, Ronen.

Outcomes