AnsweredAssumed Answered

Connecting two AD9984A with single PLL?

Question asked by pavanbabut on Apr 27, 2016
Latest reply on May 17, 2016 by DerekBurke

Wondering if I can use two AD9984A converters on a single board with one being the master PLL generator while the other one use that output (HSOUT) as HSYNC input. I will be using a single two-wire serial with the required setups on VSOUT/AO pin.

 

HSYNC0---> IC1 ---> HSOUT ---> HSYNC0 ---> IC2

 

If this is possible, how could one design the second IC with the inputs from first IC, as simple schematic would be helpful.

 

thanks

Outcomes