AnsweredAssumed Answered

Is my AD8302 fried?

Question asked by zapora.nicolas on Apr 26, 2016
Latest reply on May 6, 2016 by jdobler

Hi,

I'm using the AD8302 for phase detection, with the circuit of the figure 4 on the datasheet.

I don't have the 1.8V in the Vref, C1 C4 C6 C5 C2 C8 = 100nF, R1 R2 = 51ohms, input 4MHz between 0 and -60dBm.

But every signal that I apply on the Input, the output becomes Vcc. Even if I variate the frequency or the amplitude level of my signals, the output has Vcc.What can I do? What's the matter with my circuit?

Attachments

Outcomes