AnsweredAssumed Answered

ADXL001-70BEZ accelerations during impact the pendulum in the car headrest

Question asked by andrzej.zielinski on Apr 25, 2016
Latest reply on Apr 25, 2016 by NevadaMark

I would like to use accelerometers ADXL001-70BEZ for laboratory where we can measure accelerations during impact the pendulum in the car headrest. There is 24km/h and acceleration max. 70g during 3 seconds. Could you confirm that these sensors are suitable for this application?
We would like to use standard ISO 6487:2002 Road vehicles -- Measurement techniques in impact tests -- Instrumentation
Do you know the modules which have Butterworth phaseless digital filter?

Outcomes