AnsweredAssumed Answered

Using ADG5404F mux like a demux?

Question asked by andras on Apr 20, 2016
Latest reply on Apr 22, 2016 by ngray


Hi All,

 

We would like to use ADG5404F multiplexers to select output for a single current source. I am wondering if it is possible to connect the current source to the D pin (pin 6) and sink on the S pins (pin 4,5,10,11) with using 40V single power supply for the IC. In the datasheet I found, that S and D pins can be input and output, but it is never mentioned again, and I am not sure if the specification is the same for D to S current flow and S to D current flow.

Thanks for you advice!

ANdras !

Outcomes