AnsweredAssumed Answered

Make LDR file without zero init headers

Question asked by jbagg on Apr 20, 2016
Latest reply on Apr 28, 2016 by Kader.M

Is there a way to get the CCES Sharc linker to generate a LDR file that puts the zero data into data sections (INIT_* below) instead of zero init headers (ZERO_* below)?

 

from 489_spi.asm

0x0 FINAL_INIT

0x1 ZERO_LDATA

0x2 ZERO_L48

0x3 INIT_L16

0x4 INIT_L32

0x5 INIT_L48

0x6 INIT_L64

0x7 ZERO_EXT8

0x8 ZERO_EXT16

0x9 INIT_EXT8

0xA INIT_EXT16

 

I'm trying to debug a SPI slave booting issue and I suspect the issue is the pausing when a zero init header is sent.  I know it will make the image much larger, that is ok for this exercise.

Outcomes