AnsweredAssumed Answered

Building AD9467-FMC-250EBZ ref project

Question asked by rscavetta on Apr 19, 2016
Latest reply on Apr 22, 2016 by CsomI

Hey Guys,

 

I'm trying to build the AD9467-FMC-250EBZ reference design in:

Vivado v2014.2 (64-bit)
SW Build 932637 on Wed Jun 11 13:12:34 MDT 2014

IP Build 924643 on Fri May 30 09:20:16 MDT 2014

Copyright 1986-2014 Xilinx, Inc. All Rights Reserved.

 

I cloned the hdl repo on branch hdl_2014_r2 and started to build the library dependencies from this list:

https://wiki.analog.com/resources/fpga/docs/hdl    (Scroll down to the heading "AD9467FMC")

Unfortunately the libraries:  util_axis_resize & util_axis_fifo are not in that branch but do appear in later branches.

 

So, how is it possible to build this reference design without those libs?  Can they come from a newer version?  If so and I upgrade Vivado to a version that supports those libraries then I assume the project will no longer build because it's tired to Vivado 2014.2 with a version check.

 

I've going in circles for a week now.  Can't make sense of the version problems...

 

Regards,

Rock

Outcomes