AnsweredAssumed Answered

Is it possible to set a resolution for ADV7441A

Question asked by NanjundaM on Apr 18, 2016
Latest reply on Jun 27, 2016 by JeyasudhaMuthuPerumal

Hi,

 

I have a design in which the ADV7441A is used for DVI inputs.

I have a DVI source which will detect the sink with SXGA resolution and it will output accordingly.

 

My requirement is to implement this, how do I make the settings to ADV7441A so that it is set to SXGA resolution and it gives the details of the same to DVI source(above mentioned).

 

Is it possible to implement this with ADV7441A ?

How do I set the input resolution to SXGA and pass this information to input source ?

Is it possible to implement this with EDID configurations ?

Please help me ASAP.

 

Thanks in regards,Nanjunda M

Outcomes