AnsweredAssumed Answered

HMC611LP4E N/C pin

Question asked by sss on Apr 18, 2016
Latest reply on Apr 18, 2016 by jdobler

Hi all,

 

Which is the correct connection ?

N/C pin should be connected to GND or open ?

 

@ HMC611LP4E datasheet,

9 page

Pin Descriptions

1, 6, 7, 13,17, 18, 21, 22 N/C These pins are not connected internally.

 

11page

Application & Evaluation PCB Schematic

1, 6, 7, 13,17, 18 pin :N/C connect to GND

21, 22 pin  :N/C open

 

12 page

Evaluation PCB

1, 6, 7, 13,17, 18, 21, 22 :N/C open ?

 

Best regards,

sss

Outcomes