AnsweredAssumed Answered

Question for AD7740

Question asked by kawamata on Apr 13, 2016

Hi , I have a questioin about AD7740 (V-F converter) .

I use AD7740 with EX clock(1% accuracy).

I want to drive AD7740 with 1000kHz clock .

but , max CLKIN of AD7740  is 1000kHz .

Can I use AD7740 with silicon oscilator (1% accuracy ,1000kHz)?

So,  which FREQUENCY should I use as TYP CLKIN ? (990kHz ? in this case)

Or , it isn't so big deal , If 1010kHz clock come into AD7740?

 

So please anyone help.

Outcomes