AnsweredAssumed Answered

handling pins of ADV8005

Question asked by Kikka on Apr 12, 2016
Latest reply on Apr 13, 2016 by Kikka

Hello.

 

I have some questions how to handle pins of ADV8005.

 

1. ARC1_OUT(B7), ARC2_OUT(A7)

UG-707 says : Connect this pin to ground through a 4.7kΩ resistor if unused

The schematic of EVAL-ADV8005-SMZ says : Open

Which is correct?

 

2. HEAC_1+(M22), HEAC_1-(M23), HEAC_2+(V22), HEAC_2-(V23)

UG-707 says : Connect this pin to ground through a 4.7kΩ resistor if unused

The schematic of EVAL-ADV8005-SMZ says : Open

Which is correct?

 

3. N23 pin

Datasheet says : AVDD3(HDMI Tx1 Analog Power Supply (1.8 V))

UG-707 says : Connect this pin to ground.

Which is correct?

 

4. W23 pin

Datasheet says : AVDD4(HDMI Tx2 Analog Power Supply (1.8 V))

UG-707 says : Float this pin

Which is correct?

 

5. REF_CLK(C14), REF_HS(D14), REF_VS(D15)--from datasheet.

UG-707 says : these pins are NC.

Which is correct?

 

Thank you in advance.

 

Best regards.

Kikka

Outcomes