AnsweredAssumed Answered

ADRF6655 EVALZ...Can it be used for programmable WLAN to UHF (400-600MHz) up/down converter prototyping???

Question asked by bharathkeshavamurthy on Apr 12, 2016
Latest reply on Apr 19, 2016 by mthahira

I am building a TV White spaces prototype. I wanna know if the ADRF6655 EVALZ evaluation kit is capable of the following tasks:

1. The LO should be capable of producing frequencies of around 2800MHz-2900MHz. Is it possible?

2. The RF input to the mixer is 2412MHz (WLAN). Is it possible?

3. The LO frequency should be programmable via SPI using an FPGA/ARM processor as the controller. Is it possible?

Outcomes