AnsweredAssumed Answered

AD8429 for pH monitoring ?

Question asked by kbm10 on Apr 10, 2016
Latest reply on Apr 11, 2016 by harryh

Hi All,

I am trying to monitor pH from a low impedance sensor. The glass electrode is used as a reference.

 

The input referred noise of the amplifier needs to be low as well. AD8429 seems to be the lowest noise option. AD8421 is another option which I have not tried yet.

 

AD8429, dc-coupled at a gain of 5 was tested. However the sensor signal (between 0.1 -1 Hz) seems to be very low. The sensed signal (5 mV) is nearly a 100 times less than the expected signal ( 550 mV). Any reason why ?

Outcomes