AnsweredAssumed Answered

ADI Reference Designs HDL User Guide -- make problem

Question asked by AdrianC Employee on Apr 7, 2016
Latest reply on Apr 7, 2016 by AdrianC

got this on e-mail:

 

    When I execute command make in the directory of [hdl/library/axi_ad6676], I got problems as follows:

 

      ry/axi_ad6676'. You can use the ipx::package_project -import_files option to copy remote files into the IP directory.
299 INFO: [IP_Flow 19-2228] Inferred bus interface "rx" of definition type "analog.com:interface:fifo_rd:1.0".
300 WARNING: [IP_Flow 19-2999] Will not infer bus interface "rx" for "analog.com:interface:fifo_wr:1.0". The interface exists with different type "analog.com:interface:fifo_rd:1.0".
301 ERROR: [Common 17-55] 'set_property' expects at least one object.
302 Resolution: If [get_<value>] was used to populate the object, check to make sure this command returns at least one valid object.
303 INFO: [Common 17-206] Exiting Vivado at Wed Apr  6 22:22:20 2016...
"axi_ad6676_ip.log" 303 lines --100%--    

Also when I execute command make in directory [hdl/projects/fmcomms1/zed], I got error as follows:

710 ERROR: [BD 5-216] VLNV <analog.com:user:axi_clkgen:1.0> is not supported for the current part.
711 ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

712
713     while executing
714 "create_bd_cell -type ip -vlnv analog.com:user:axi_clkgen:1.0 axi_hdmi_clkgen"
715     invoked from within
716 "set axi_hdmi_clkgen [create_bd_cell -type ip -vlnv analog.com:user:axi_clkgen:1.0 axi_hdmi_clkgen]"
717     (file "../../../projects/common/zed/zed_system_bd.tcl" line 118)
718
719     while executing
720 "source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"
721     (file "system_bd.tcl" line 2)
722
723     while executing
724 "source system_bd.tcl"
725     (procedure "adi_project_create" line 97)
726     invoked from within
727 "adi_project_create fmcomms1_zed"
728     (file "system_project.tcl" line 6)


Since my vivado version is 2015.4, so the problem may be caused by version of vivado. Is convenient for you give any suggestion or tcl files that can help me solve this problem?

Outcomes