AnsweredAssumed Answered

Bulk USB communication using CLD example project

Question asked by SJ.KIM on Apr 4, 2016
Latest reply on Apr 29, 2016 by SJ.KIM

Hello everyone here,

I am trying to do bulk USB communication using "CLD_Bulk_loopback_Ex_v1_1" project provided by CLD company

on the the BF707-ezkit board.

In the CCES 2.2.0, the CLD_Bulk_loopback_Ex_v1_1 project is successfully built.

And, I run the hostapp.exe in the DOS command window.

For the -v option(hostapp-v), it works successfully and printout the correct results.

please, refer to figure 1 in the attached file.

But, the -a option(hostapp-a), it does not works successfully, it printout some error messages.

please, refer to figure 2 in the attached file.

Also, the -l option(hostapp-l), it does not works and printout error messages.

please, refer to figure 3 in the attached file.

The hostapp project has been built again in the VS2013. But, the results are same.

(I am using Windows 10)

If anyone has the same experiences and have clue to solve the problem, I am looking forward to

sharing your experience.

If the above information is not enough, please, let me know.

Thank you in advance.

Attachments

Outcomes