AnsweredAssumed Answered

ADC Requriement

Question asked by SHARVY on Apr 3, 2016
Latest reply on Apr 26, 2016 by SHARVY
Branched to a new discussion

I am having a latest requirement to design the new ADC cards with the below specification. Kindly let me know, about which ADC chip from AD is more suited.

 

  • Type
    1:
    • Analog inputs: Minimum, 8-Analog
      Inputs (AI) w/ Surge Protection. Surge protection shall be external.
    • Resolution: 10-12bit, min
    • Precision: +/- 0.5% on DC Readings
    • Channel Isolation: 1000 Volts
      isolation between each channel
    • Input Impedance: Min 20 mega ohms up
      to 350 volts ranges, 230k Ohms up to 100 mv range.
  • Type 2:
    • 4-20mA

 

Best Regards

Sharvy

Outcomes