AnsweredAssumed Answered

ADP3050 - configure into non-inverting buck-boost

Question asked by Diaane on Apr 1, 2016
Latest reply on Apr 7, 2016 by Diaane

ADP3050 is a buck regulator. I saw in the datasheet that it can be configured as buck, buck-boost, and SEPIC regulator. In the datasheet also there is a reference design for an inverting buck-boost. My question is, is it possible to also configure it to non-inverting buck-boost? If yes, how?

 

Also, it is written on the Product Info page that there are newer alternatives available for ADP3050, which are ADP2441 and ADP2442. Are these chips configurable to non-inverting buck-boost?

 

Lastly, do you have any chip which is step down with input range of 5-60V  to 12V output? Is that chip configurable to buck-boost?

Outcomes