AnsweredAssumed Answered

DVI Script Issue with EVAL-ADV7842-7511P

Question asked by wood0201 on Jul 8, 2011
Latest reply on Aug 5, 2011 by GuenterL

I have an EVAL-ADV7842-7511P setup with DVI from a pattern generator feeding it over an HDMI cable.  I am outputting DVI over an HDMI cable to my monitor.  I run the DVI script - "DVI RGB In, RGB Out DVI" and I get a blue screen output at 640x480/60 no matter what resolution I use on the input.  Does this type of output indicate the input is not being recognized at all?  Am I running the correct script?  Do I need to perform something else in addition to make this work?

 

I know the board is function because I can put in multiple analog RGB resolutions, run the associated script, and get the proper DVI output to my monitor.

 

Thanks,

Nathan

Outcomes