AnsweredAssumed Answered

ADZS-SC589-EZLITE boot from ROM and external memory?

Question asked by Hans3 on Mar 30, 2016
Latest reply on Mar 31, 2016 by Harshit.Gaharwar


Hi, are there two ways to load a program in ADZS-SC589-EZLITE? One in the internal ROM and second in the SD card?

In POST example, it says "showing how to program the POST test into flash memory for the ADSP-SC589 EZ-Board are given below" does this mean the external SD card? or there is an external flash? Because, SC589 does not have internal flash.

If one can use internal ROm which i think is 320kB to load, why there is a need for external flash?

Outcomes