Niels

Channel Protection Device in tiny Package

Discussion created by Niels on Mar 30, 2016
Latest reply on Apr 8, 2016 by Niels

Hello all,

I think you all know the famous channel protection devices from AD. Starting with the AD467 / ADG465, and followed by the ADG5462F.

All of the have two common attributes:

- they are fantastic devices

- they come in quite huge packages

I wonder if it is possible to build some kind of 4 channel ADG467 in a UDFN10 package.

The UDFN10 package is common for TVS diode arrays. It allows a nice pass-through pinout and is only 2.5 x 1.0 mm. This would be really cool stuff.

Do you agree?

 

I am looking forward to your answers.

Regards, Niels

Outcomes