AnsweredAssumed Answered

AD9650: VCM pin

Question asked by Mr.K on Mar 28, 2016
Latest reply on Apr 12, 2016 by PMH

Hello,

 

I have a question about the VCM pin of the AD9650.

I am using the AD9650 by the configuration like Figure 79 in the AD9650 datasheet.

In my circuit, the VCM of AD9650 operates abnormally.

 

AS for the operation, the VCM does a continuous toggle to the High/Low level(1.8Vp-p).

When the VCM disables servo bit clearing 0x0F register of the AD9650, 1.8V level is output from the VCM.

I confirmed the VCM of AD9650 with the ADC driver cutting it.

However, the behaver of VCM did not change.

 

Could I have advice of the cause of this problem?

 

Best Regards,

Mr.K

Outcomes