AnsweredAssumed Answered

Question about the ADL5380 RX EVM

Question asked by Matt1012 on Mar 25, 2016
Latest reply on Apr 4, 2016 by stanis

Hi,

As I checked the datasheet of ADL5380 and saw the RX EVM in Figure 87  which shows the zero-IF EVM performance of a 10 MHz IEEE 802.16e WiMAX signal through the ADL5380. Is there any similar performance result based on 10MHz or 20MHz LTE 64QAM signal?

 

The another question is " will the sampling rate affect the EVM value?  "

Is there any similar performance result based on 100MSPS & 200MSPS sampling rate ?

 

Thanks.

Matt

Outcomes