AnsweredAssumed Answered

AD8036 Clamping Amplifier Accuracy over Temperature

Question asked by smacleod on Mar 22, 2016
Latest reply on Jun 25, 2016 by iamPhil

The AD8036 has typical input offset and offset tempco specified as 2 mV and 10uV/C, respectively.  And the clamp accuracy is 3 mV typical.  Is there a tempco spec available for the clamp accuracy?  Also, is there a hysteresis spec for the clamp performance?  My application is for DC and low frequency signals of less than 1 kHz.

 

Thanks,

Steve

Outcomes