AnsweredAssumed Answered

Selection of audio amplifer

Question asked by Sayantan on Mar 21, 2016
Latest reply on Mar 21, 2016 by iamPhil

Dear support team,

 

I need two audio outputs of below specifications:

1. able to drive 600 ohm load at 12V RMS output voltage level.

2. able to drive 150 ohm load at 15V RMS output voltage level.

I am using ADAu1916 audio codec which is giving 0.92V rms output & working on 3.3v single ended voltage rail, I need to amplify it to meet my requirement. Please suggest me some amplifier to meet my requirement.

 

Regards,

Sayantan

Outcomes