AnsweredAssumed Answered

Errors while creating the FMCMOTCON2 reference design

Question asked by qxj on Mar 17, 2016
Latest reply on Mar 18, 2016 by qxj

Hi,

 

After running the command 'source ./system_project.tcl' on the TCL console, the reference design FMCMOTCON2 (hdl_2014_r1) was being automatically created.

 

But after a few time, some errors appeared saying that:

 

 

 

ERROR: [BD 5-216] VLNV <analog.com:user:util_adc_pack:1.0> is not supported for this version of the tools.

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

 

    while executing

"create_bd_cell -type ip -vlnv analog.com:user:util_adc_pack:1.0 current_monitor_m1_apack"

    invoked from within

"set current_monitor_m1_apack [create_bd_cell -type ip -vlnv analog.com:user:util_adc_pack:1.0 current_monitor_m1_apack]"

    (file "../common/motcon2_fmc_bd.tcl" line 131)

 

 

    while executing

"source ../common/motcon2_fmc_bd.tcl"

    (file "system_bd.tcl" line 3)

 

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 97)

    invoked from within

"adi_project_create motcon2_fmc_zed"

    (file "./system_project.tcl" line 6)

 

 

 

In the past I successfully built the reference design for many times, so I wonder why it failed this time.

 

I'm sure that I have built all the necessary libraries and the version of Vivado is 2014.4.1.

 

Regards,

qxj

Outcomes